2018-04-16 02:37 PM
What is the magnetic rms noise of the LSM9DS1? I can not find it or something simular in the datasheet. Thanks for your help.
#magnetic-rms-noise2018-04-16 11:38 PM
Magnetometer part of LSM9DS1 is basically the same as LIS3MDL.
2018-04-30 12:09 PM
Thanks for your answer. These sensors have zero gauss levels of +/- 1 gaus which is a quater of full scale. Is that correct ? Why not all of your sensors have that offset compensation to reduce the zero gauss level.
Regards,
Ralf L
2018-05-02 02:57 PM
Yes, it is correct.
In the final application, there is always some hard iron distortion caused by surounding objects which need s to be compenstated. The zero gauss level will be compensated together with the HI distortion, so it is not a big problem.