cancel
Showing results for 
Search instead for 
Did you mean: 

LSMDSOX + Profimems ((STEVAL-MKI109V3)

pauljainta
Associate

I have been trying to log data using LSMDSOX + Profimems, but it does not record any data. I have attached pictures of this. I have not updated the firmware, and I am using Ubuntu 22.04. I have exported the data to a file, and it is empty. 

 

Screenshot from 2024-08-29 15-52-04.pngPXL_20240829_221637248.jpgScreenshot from 2024-08-29 15-54-59.pngScreenshot from 2024-08-29 15-52-04.png

 

3 REPLIES 3
Federica Bossi
ST Employee

Hi @pauljainta ,

Are you using the latest version of MEMS Studio?

Do you always get the error that the sensor was not recognized?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
pauljainta
Associate

Hi @Federica Bossi , I used version 1.3.0. I could not upgrade the firmware, and I get the error about 2 out of 5 times. When the error does not show up, I cannot see any data in the data monitor. 

Hi @pauljainta ,

It is very strange, could it be that the adapter is not inserted properly? Do you have any others to see if you are still experiencing the same problem?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.