2018-07-26 09:30 AM
I am using a LSM9DS1, the datasheet doesn't clearly state the settings for HPF cutoff for accelerometer.
Moreover, when I enabled HPF using Reg7_XL, I get 0.18g on all the axis, which is noise since my platform is stable. Can somebody help me with this?
2018-08-09 08:46 PM
@ST Community who is covering MEMS?
2018-08-10 04:47 AM
@Nerd can you share you sensor configuration?
What do you write to CTRL_REG7_XL to enable HPF?
2018-09-23 08:20 AM
DCF[1:0] set to 10
FDS set to 1
Rest of the bits are all 0
2018-09-26 01:36 AM
The high pass configuration is correct.
The noise cannot be 0.18g, I guess you misinterpret the output date or you have another mistake in your code.