LSM9DS0 and LSM9DS1 acceleration sensitivity confusion
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-12 5:49 PM
All the sensitivity values for the acceleration fit within 16 bits, however �16 g does not.
Let�s use FS �2 g as an example sensitivity level. As the range is -2 to +2, this would be a total of 4g. Or 4,000 Milli-Gs.
The output is 16 bits. 16 bits equals 65,535. This means we can get 65,535 different readings for the range between -2 and +2. (or -2,000 MilliGs and +2,000 MilliGs)4,000 MilliGs / 65,535 = 0.061
0.061 is what is seen in the datasheet for
�2
here are the values for all sensitivity levels;
�2 =
4,000 MilliGs / 65,535 = 0.061
�4 =
8
,000 MilliGs / 65,535 = 0.122
�6 =
12
,000 MilliGs / 65,535 = 0.183
�8 =
16
,000 MilliGs / 65,535 = 0.244
�16 =
32
,000 MilliGs / 65,535 =
0.488
The only one that doesn't match up with the datasheets for both LSM9DS0 and LSM9DS1 is for
�16. The calculations above show 0.488, but the datasheets have 0.732
Can someone please explain why this is so?
#lsm9ds1 #accelerometer #lsm9ds0- Labels:
-
Accelerometers
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-13 4:01 AM
It is not uncommon that the output values doesn't cover the whole 16-bit range of output registers. From that reason the sensitivity is listed in the datasheet.
Basically it means that the resolution is lower than 16-bits.
You have to use the sensitivity mentioned in the datasheet to get correct acceleration value.