2022-08-25 07:58 AM
I'm trying to use several different IMUs in the LSM6DS family (LSM6DSOX and LSM6DSO32). Both of them are exhibiting "ringing" on the three gyro axes when exposed to shock (knocking the PCB against a table). It almost looks like there's no anti-aliasing filter, but as far as I can tell, I've enabled LPF1. Any insight here? Things to check?
See attached graph of gyro X data.
Configuration:
Thanks.
2022-09-02 07:39 AM
Hi @JimJ ,
Did you try also bypassing the FIFO, i.e. in continuous mode (with he BDU bit enabled), and check if you can reproduce the same issue?
-Eleon