cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSV - temperature issue

AlexBT
Associate

Hello,

I am trying to get the temperature from LSM6DSVX sensor. Accel and gyro are working well but I can't get the temperature. The buffer cannot be enable for temperature. It works for Accel  and gyro buffer can be enable.

their is something specific to do for the temperature ? 

 

cmd line :

echo 1 > /sys/bus/iio/devices/iio:device3/buffer/enable

return : 

write error : invalid argument.

3 REPLIES 3
ASoni.2
Associate III
chamois94
Associate

Any help on this please ?

Federica Bossi
ST Employee

Hi @AlexBT , @chamois94 ,

You can try to implement our official drivers where the temperature reading is included.

Let me know if this helps :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.