cancel
Showing results for 
Search instead for 
Did you mean: 

GUI Error with Camera 16GZMAI

SeanF
Associate

Hi,

I am experiencing a technical issue with the ST 16GZMAI camera when connected to the EVK-U0I1 control board.

While the system works fine with my 55G1MBI1 camera, the EVK GS 1.1.2 GUI fails to recognize this specific model and displays the following error:

"Error: could not broadcast input array from shape (341,280) into shape (340,280)"

I am also unable to change the detector format. Could you please refer me to a technical expert who can assist with the configuration of this model?

Best regards,

Sean

3 REPLIES 3
Jean_Poire
ST Employee

Hi @SeanF ,

This is a known bug; it has already been fixed and will be soon released in the next GUI version.

I will let you know as soon as the new GUI is available.

Sry for the troubles,

Best regards,

Jean 

Hi again,
I wanted to ask if there’s any update on when the updated GUI version will be released. I need to use this camera for my degree project, so I’d really appreciate any timeline you can share.

Jean_Poire
ST Employee

Hi @SeanF ,

I can't give you a schedule about the release. I can only suggest you to work meanwhile with our python sdk solution : STSW-IMG507 | Product - STMicroelectronics

 

Best regards,

Jean