LSM6DSO not reading 1G at rest
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-08 2:47 PM
I am writing my own library in C++ to operate the LSM6DSO and when the sensor is at rest it reads 0.5 G on the z-axis, I've tried the code with 2 ICs, one in an Adafruit breakout board, and another one in an old PCB that had the sensor soldered one and both got the same error, so I believe that the issue might be in the code, but I can't identify where is the problem. Btw, I am using the dev kit NUH7AZIQ$ATZ3A140012 (STM32H7A3ZIT6Q). Also, when i turn the sensor 90 deg the 0.5g moves to the other axis, and regardless of the range scale I choose, the readings adjust themselves so that it still gives the 0.5 G after applying the conversion factor .
The first line shows the reading from the CTRL1_XL register and breaks it down into the configurations in that register (which in this picture is set up to +-2G range and sampling of Hz)
the second lines show the reading from the OUTZ_L_A (2Ch) and OUTZ_H_A (2Dh) registers, then it combines that into the raw data and multiply by the sensitivity factor suggested in the data sheet for each range ( in this case 0.0061)
Small programs that plots the lsm6dso outputs, as I turned the imu, the 0.5 g readings moved to the other axis
Here is the part of the code, in this section I its not exactly the library i am writing but it has follows the same procedures and gets the same numbers.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-01 9:58 AM
I fixed the thing you mentioned, and the behaviour of the Gyroscope changed a lot; now it seems to be more sensitive, but I guess it's still within a reasonable range. And it didn't change anything for the accelerometer
Now the ADDR : 0x11 (CTRL2_G) = 0x42
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-03 8:54 AM
No more ideas on what could be wrong. LSM6DSO has been in production for years now and there are no known issues with the HW or with the official standard C drivers.
Last question: did you write to some wrong register address? (there are few undocumented register addresses which hold the factory calibration including the sensitivity and if you happen to write them then the sensor will not behave correctly and calibration will be compromised)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-04 11:36 AM
Can you double check that you are using LSM6DSO?
If you are using LSM6DSO32 then the '01' full scale bits would correspond to 32g and then the conversion factor would be 0.976 which would give you the right values
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-05 5:25 PM
The ic is on a old breakout board used by our team, so I can't ensure that no one wrote to any unlisted address.
Also, this breakout board was bought from adafruit and its listed as lsm6dsox, which according to their datasheet is the lsm6dso not the lsm6dso32.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-06 8:47 AM
Understood. The WHO_AM_I register is the same in both cases. However, because we are now sure that configuration is correct because we have read it back, and we are sure that int16 values are read correctly, we can conclude that you are using LSM6DSO32 or LSM6DSO32X.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-12 6:51 PM
I am using this breakout board https://www.adafruit.com/product/4438 to write and test code, in adafruit website they state it's an LSM6DSO, not the 32-bit version. So, I am looking into buying a new breakout board. I will wait until I can test the code on it and let you know if that fixes the issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-13 8:44 AM
(side note: 32 in the part number means 32g max full scale, not 32 bit)
I can see that the link you sent point to a board where they say LSM6DSO with max 16g full scale is utilized - nevertheless after ruling out all possible errors we can only conclude that you are using LSM6DSO32, the variant with 32g max full scale.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-13 8:47 AM
In the page you have linked, there is a link to the schematic overview: Overview | LSM6DSOX, ISM330DHC, & LSM6DSO32 6 DoF IMUs | Adafruit Learning System
In that page they confirm that there is a variant of your board that indeed utilizes LSM6DSO32 ! You probably have this variant (the so-called "industrial" variant)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-13 9:22 PM
In the breakout board itself is written LSM6DSOX, but i guess at this points it's worth testing it the code the 32g variant

- « Previous
-
- 1
- 2
- Next »