cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSL big gyroscope fluctuations on acceleration

AnselmeC1
Associate

Hello,

 

I am using a LSM6DSL sensor and when applying a 2G acceleration without rotating the board, I get very important spikes on the gyroscopes of about -90°/s to +90°/s amplitude.

This is very strange. Is this a normal behaviour from this sensor ? Are there settings or ways to avoid this ?
I noticed the exact same behaviour on the LSM6DSV16X sensor.

Thank you for your help

1 REPLY 1
Federica Bossi
ST Employee

Hi @AnselmeC1 ,

Have you enabled the BDU bit in register CTRL3_C (12h)? If not, can you please try?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.