2018-06-21 8:23 AM
Dear all,
I'm working on a LSM6DS3 chip.
I have configured it to exploit the Activity/Inactivity recognition functionalities, and all is working.
On the other hand, I'm not able to do the following and/or to find documentation references for that.
The chip recovers
from the Inactivity state to the fully Active state if I shake it or tap it, which is fine.
But I would like to restore the fully Active state by software, without the need of physically touching the sensor.
Is there any way this can be achieved?
I tried resetting registers, re-configuring and so on, but this seems not to be working.
Thanks for help and hints.
Cheers,
Roberto
#accelerometer #lsm6ds3 #power-saving2018-07-27 12:04 AM
You should be able to switch from inactivity to activity mode by writing: