2018-10-23 04:04 AM
If I want to test the LPS33HW and I already have the X-NUCLEO-IKS01A2 motion MEMS place over STM32 Nucleo test by DataLogTerminal SW from X-CUBE-MEMS1 package.
I see there is LPS33HW EV STEVAL-MKI183V1. But I didn't see any reference to use it on the X-NUCLEO-IKS01A2 (also it look compatible in pins location), and no SW or user guide how to test them together.
2018-10-23 08:09 AM
Please check X-CUBE-MEMS-XT1 package which support sensord connected in DIL24 socket on X-NUCLEO-IKS01A2.
In this package you can find DataLogTerminal which sends data to serila terminal and DataLogExtended which copoperates with grpahical tool Unicleo-GUI.