cancel
Showing results for 
Search instead for 
Did you mean: 

LPS25HBTR pressure reading decreasing over time

2067
Associate II

I have bought a MKI-165V1 to test LPS25HBTR,but I find that the pressure value is decreasing for a long time ,from 1014.117 to 1002.970 in an hour.It is not stable,the next is my initial code,what is the reason for it

uint8_t data = 0x90;
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x20 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
HAL_Delay(10);
data = 0x00;
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x21 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
// HAL_Delay(10);
// HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x22 , I2C_MEMADD_SIZE_8BIT, pData, Size, 0xFF);
HAL_Delay(10);
HAL_I2C_Mem_Write(&hi2c4, 0xB8, 0x23 , I2C_MEMADD_SIZE_8BIT, &data, 1, HAL_MAX_DELAY);
HAL_Delay(10);
10 REPLIES 10
Federica Bossi
ST Employee

Hi @2067 ,

Can you please implement our official drivers and let me know if you still have the problem?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I think this sensor doesn't have many registers, so there's no need to use the official driver. Are there any other reasons for this, or are there any stable sensor configurations you would recommend?

Hi @2067 ,

It was just a way to check that your fw was correct.

Do you have a reference sensor with which you measure humidity?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I am measuring atmospheric pressure with the sensor, and I am currently taking measurements at an altitude of 120 meters indoors. However, without a reference firmware, I have noticed that the sensor readings can vary by more than 10 hPa in the same environment. I would like to know what might be causing this.

Hi 2067,

Would it be possible for you to run two identical development boards with your software in the same environment and to compare the results? Can you read sensor's internal temperature?


I don't have two  boards; I only have one MKI-165V1. This sensor has temperature compensation, and I haven't tried to read the temperature.

How do I use the RPDS registers, and how can I implement the One-Point Calibration feature? Does this chip come with temperature compensation? Can the factory-set parameters affect the output?

I don't have two  boards; I only have one MKI-165V1. This sensor has temperature compensation, and I haven't tried to read the temperature.

How do I use the RPDS registers, and how can I implement the One-Point Calibration feature? Does this chip come with temperature compensation? Can the factory-set parameters affect the output?

Hi @2067 ,

You don't need an external compensation since the device is already internally compensated over temperature. And this can't affect the humidity parameter.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Old_Geezer
Associate III

Hi 2067

That drift can be attributed to both weather wind and ventilation.

But to find what is weather, what is drift, what is noise, make a science project of it!

1 Get your grandma's biggest preservation jar and put your device in it

2 If you have an analogue barometer put it there as well, it will likely show a constant offset to your device.

3 Program your device to make ten samples or more per hour for 24 hours. You'll see both drift and noise level.

4 Watch out for any heating on the sensor.

5 Watch out for windy days as air pressure on the facade makes readings wobbly.

6 And close the lid, make it air tight with soap, and have it all in shadow. Maybe in the basement.

7 Do regular analogue readings too, if you had a barometer

And please show the results here :)

If your readings differ from the local digital weather report, then you and ST can start a discussion!