cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3MDL Temperature problem.

TBart.1
Associate II

Hello. We know that lis3mdl is temperature sensitive, i.e. there is a scale shift. From what we have read, this cannot be compensated for with software ( Or maybe it's possible? ). Therefore, can this be prevented physically, e.g. by using some thermal paste? The idea is to prevent lis3mdl from heating up too much. Our operating temperature range is 10-35 degrees Celsius. Thanks.

2 REPLIES 2
AScha.3
Chief II

Hi,

>The idea is to prevent lis3mdl from heating up too much.

from ds:

AScha3_0-1721559152682.png

The lis3 heating up at 0.6 mW power consumption ? (at its nominal 2.5V supply)

No, never... almost impossible, to get any temp.rise to measure, i think.

btw :   at which voltage you use it ?

If you feel a post has answered your question, please click "Accept as Solution".

It's not about the voltage heating up, it's about the external ambient temperature.