2023-06-09 08:46 AM
Hello,
I want to use the LIS3MDL for a project. I am using a microcontroller with I2C lines at 3V3. In the datasheet there is mentioned that the typical voltage for VDDIO is 1V8 but with a range up to VDD +0.1 V. I will power the device (VDD) with 3V3. If I also use 3V3 for the VDDIO will the sensor communicate at 3V3 or 1V8.
Thank you in advance
Solved! Go to Solution.
2023-06-09 12:14 PM
Welcome, @Noah Verstraete, to the community!
Correct, you can operate VDDIO with the same voltage as VDD, if VDD=3.3V.
The sensor always communicates on the level of VDDIO, in this case with 3.3V.
Does that answer your question?
Regards
/Peter
2023-06-09 12:14 PM
Welcome, @Noah Verstraete, to the community!
Correct, you can operate VDDIO with the same voltage as VDD, if VDD=3.3V.
The sensor always communicates on the level of VDDIO, in this case with 3.3V.
Does that answer your question?
Regards
/Peter
2023-06-12 12:55 AM
Yes, thank you for clarifying.
Best regards
2023-06-12 06:44 AM
You're welcome!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter