2019-08-05 7:27 AM
hi stm,
i have studied lis3dsh app note,
i didn't understand complete configuration for wakeup state machine , like after setting the registers to the specific value , interrupt will be generated , how to make it periodic interrupt , what are all the things need to be done to get an interrupt from wakeup can anyone please explain briefly , like what i need to do if i want to configure wakeup state machine.
Regards,
Manjunath
2020-11-28 10:35 AM
Did you ever get it sorted out? I'm having the same issue, my state machine only triggers INT1 once and I have no idea why. The command 11h should return the state machine to the start but looks like it doesn't. I followed the APP note A3393 and the wake up example.