cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH12TR- Not working on 3.3V.

Smalik
Associate II

Hello,

I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greater than 2.8V?

Any help would be appreciable

Thanks and Regards

Sarthak Malik

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @Smalik (Community Member)​ ,

let's keep only this thread active.

-Eleon