2022-10-19 10:53 PM
Hello,
I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greater than 2.8V?
Any help would be appreciable
Thanks and Regards
Sarthak Malik
2022-10-20 3:37 AM
Hi Sarthak Malik @Smalik ,
Are you using the Vdd and VddIO together?
-Eleon
2022-10-28 12:24 AM
Hello Eleon @Eleon BORLINI
Sorry for the delayed response actually the Diwali holidays were going on that's why I am unable to reply.
Yes, I am using the Vdd and VddIO together.
Thanks
Sarthak
2022-11-02 12:01 AM
Hello @Eleon BORLINI ,
I hope you are doing well.
Can you please help me out in this case? I am waiting for your response.
Thanks
Sarthak
2023-01-16 12:27 AM
Hello,
I am waiting for the update. please help to use this IC on 2.9V to 3.3V.
Any help would be appreciable
Regards
Sarthak Malik
2023-01-17 5:53 AM
Hi Sarthak Malik @Smalik ,
sorry for the delay in my answer. The parts should have no issue in this sense, since we never encountered this kind of limitation and they are tested 100% at 3.6V. Which is precisely the condition you are operating? Is the application processor capable to read at that voltage? Could you try also to lower VddIO with respect to Vdd?
-Eleon
2023-01-19 4:54 AM
Hello Eleon BORLINI,
Yes, the processor is capable to read the 3.6V and we have other sensors as well on the same board which is working on 3.3V. and we can not try to use lower VddIO because it is by default short by the Vdd in our board.
Thanks
Sarthak Malik
2023-01-19 10:43 PM
Hello Eleon BORLINI @Eleon BORLINI ,
I am waiting for your answer.
Regards
Sarthak
2023-01-20 6:53 AM
Hi @Smalik ,
you might try another part if this one is not working.
-Eleon
2023-01-24 3:41 AM
Helo Eleon @Eleon BORLINI ,
Thanks for the update. Is there any problem related to this part? Because I have manufactured 100k boards by using this IC. Please provide me with the correct resolution.
Thanks
Sarthak Malik