2019-04-24 6:33 AM
Hi,
I have couple of question on LIS2DH12TR .
I'm trying to interface with CC1310 Custom Board.
1. As per the data sheet it says it doesn't need any manual calibration since factory calibration already done.( Previously have used MPU6050 didn't know much about calibration and got to know this MPU6050 has to be calibrated before use) So this LIS2DH12TR need to be calibrated before first time use?
2. I have read this sensor has an exceptional feature that sleep to wake-up and vice versa.
In my case sensor there'll be some threshold value set for vibration if there's any change in threshold value it will be sent to main controller and data will be sent over the RF.
As i assume this sensor has to be in wake-up mode all the time.
But in case of sleep mode, how will it(sensor) come back to the wake-up mode are there any external timer required to do so?
3. Since I'm not good at coding, Are there any example code for interfacing LIS2DH12TR with CC13xx series Sub-GHz.
2019-05-10 7:57 AM
Hi
Regards