LIS2DE12 no interrupt and constant acceleration values
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-09 9:31 AM
Hello,
Firs of all thank you for your time.I'm currently working with a LIS2DE12 for its great low power current but unfortunately I'm not able to get any useful information from the device. I tried to active an interrupt in the idea to check movement in any direction (i just want an interrupt if the device is moving). It doesn't work but worst when I read the register of the acceleration i have always the same values (exactly the same even when moving, reversed, ...). I guess I have made some mistakes in my configuration but I was not able to find where is the problem.Just below my pseudo-code. The I2C function are working correctly (I'm able to communcate with the
LIS2DE12 )
init:Check ACCEL_WHO_AM_I
write 0xC0 ACCEL_TEMP_CFG_REG // enable the measure of the temperaturewrite 0x57
CTRL_REG1 // 100Hz & activate all the axeswrite 0x00
CTRL_REG2 // No filterwrite 0x00
CTRL_REG3 // No specific interruptwrite 0x80
CTRL_REG4 // BDU activated for the temperaturewrite 0x08
CTRL_REG5 // Latch interruptwrite 0x00
CTRL_REG6 // no INTERRUPT on int2write 0b00101010
INT1_CFG // Interrupt OR when over thresholdwrite 0x16
INT1_THS // Set the thresholdwrite 0x03
INT1_DURATION // Set the duration (small one)write 0x00 FIFO_CTRL_REG // bypass modeloop:
check if data available ( read STATUS_REG_AUX) thenread ACCEL_OUT_X_H,ACCEL_OUT_Y_H,ACCEL_OUT_Z_H
check if INT1 == 1 then
LED = 1 // to be able to see the interruptionI hope that I respected the rules of this forum.kind regards,Denis- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-10 2:06 AM
The STATUS_REG_AUX contains an information if new new temperature data are available, you should check STATUS_REG (27h) to get the information if new acceleration data are available and then read them.
You can also share your complete code so I can check it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-10 4:35 AM
Hi,
Thx for your quick reply. I made a mistake in my pseudo code above I check STATUS_REG in my code.To be honest my code is quiet the same than the one above.main(){
accelerometerInit(); // where all the config are made (pseudo code above)
while(1){ while(!isAccDataAvailable()); // checl STATUS_REG delay(100); accelerometerAcquire(&ax,&ay,&az); delay(100); if(INT1){ // check the interruption pin yellowOn(); interruptClear(); delay(500); } else ledOff(); }}
char isAccDataAvailable(){
unsigned char a = i2c1_read1ByteRegister(ACCEL_ADDR, ACCEL_STATUS_REG); return ((a & 0x0F) == 0x0F);}void accelerometerAcquire(float *x, float *y, float *z){
delay(10); *x = convertAccel( i2c1_read1ByteRegister(ACCEL_ADDR, ACCEL_OUT_X_H) ); delay(10); *y = convertAccel( i2c1_read1ByteRegister(ACCEL_ADDR, ACCEL_OUT_Y_H) ); delay(10); *z = convertAccel( i2c1_read1ByteRegister(ACCEL_ADDR, ACCEL_OUT_Z_H) );}void interruptClear(){ // Read the INT1_SRC to clear the interruption if triggered.
i2c1_read1ByteRegister(ACCEL_ADDR, ACCEL_INT1_SRC);}The configuration above are correct for my purpose ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-11 8:50 AM
Can you please disable BDU (w
rite 0x00 to
CTRL_REG4) and try it?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-11 5:27 PM
I am having the same problem. My goal is to continually receive interrupts (level changes) on the INT1 pin any time the device is moving, however I'm not receiving any interrupts at all. I must have an error somewhere, can you please point me in the right direction? I've set my processor to detect any level change on its interrupt pin that is connected to the LIS2DE12 INT1 pin, then I am applying the values below to the LIS2DE12. The INT1 pin never changes level. Can you tell me if I should pull the pin up or down externally, and do I need to do anything else to get a level change on the INT1 pin when the device moves?
write_register_value(CTRL_REG1, 0x57); // Turn on the sensor, enable X, Y and Z, ODR = 100Hz
write_register_value(CTRL_REG2, 0x00); // High-pass filter disabledwrite_register_value(CTRL_REG3, 0x00); // No specific interrupt write_register_value(CTRL_REG4, 0x00); // FS = +/- 2g, disable BDU write_register_value(CTRL_REG5, 0x08); // Interrupt 1 pin latched, must read INT1_SRC (0x31) to clear itwrite_register_value(INT1_THS, 0x16); // Very low threshold, 0 = default write_register_value(INT1_DURATION, 0x03); // Minimum event durationwrite_register_value(INT1_CFG, 0x2A); // 00101010b, Interrupt OR when over threshold write_register_value(FIFO_CTRL_REG, 0x00); // bypass mode- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-12 3:10 AM
It's working, i guess there is a problem in reading part and it's not counted as a block read.
I will now investigate the interruption part.Thank you for your support,Denis- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-12 3:24 AM
Hello,
According to the datasheet the ''LPEN'' must be set to 1.
You should write 0x5F in the REG1, as I understand it.
I hope it will help you, but as it's not working for me I doubt.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-12 8:52 AM
Thank you for pointing that out. I gave it a try, but unfortunately it did not make a difference. Please post back if you get it working and I will do the same.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-12 10:02 AM
I've got it working! Using the settings below, when I read the INT1_SRC register I can see the bits changing as I move it around, and if I either leave my processor interrupt pin floating or pull it low, I will get an interrupt from the LIS2DE12 on the INT1 pin when motion occurs. Reading the INT1_SRC register clears the interrupt until motion occurs again. I hope this helps!
write_register_value(CTRL_REG1, 0x5F); // Turn on the sensor, enable X, Y and Z, ODR = 100Hz
write_register_value(CTRL_REG2, 0x00); // High-pass filter disabled write_register_value(CTRL_REG3, 0x40); // Interrupt activity 1 drive to INT1 pin write_register_value(CTRL_REG4, 0x00); // FS = +/- 2g, disable BDU write_register_value(CTRL_REG5, 0x0C); // Bits D4D_INT1, LIR_INT1 - 4D detection enabled (requires 6D bit on INT1_CFG), Interrupt 1 pin latched, must read INT1_SRC (0x31) to clear it write_register_value(INT1_THS, 0x16); // Very low threshold, 0 = default write_register_value(INT1_DURATION, 0x03); // Minimum event duration write_register_value(INT1_CFG, 0x7F); // All except AOI bit write_register_value(FIFO_CTRL_REG, 0x00); // bypass modefor(;;){
regVal = read_register_value(INT1_SRC); // See the bits change here as you move it around
delay_ms(200);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-12 11:28 AM
After some more fiddling, it might not be necessary to read the INT1_SRC register to receive another interrupt on the INT1 pin with motion.