cancel
Showing results for 
Search instead for 
Did you mean: 

L3G4200D INT voltage and PP_OD

michaelmichael9138
Associate II
Posted on July 03, 2016 at 07:07

What is the maximum voltage of the L3G4200D INT1 pin (assuming open drain)?

What does the PP_OD bit in CTRL_REG3 control - INT1 only or INT1 and DRDY/INT2?

What are the maximum voltages applied to all I/O pins?

Why are ST's datasheets SO BAD?  This part has been in

production for 6 years.  There's no excuse for not documenting it.

#l3g4200d
1 REPLY 1
louda.marian
Senior
Posted on July 14, 2016 at 10:02

Maximum allowable voltage applied to the INT pins is Vdd_IO + 0.3V even if it is open-drain configuration.

I will ask expert.

Maximum allowable voltage applied to any I/O pin is Vdd_IO + 0.3V.