2023-11-27 1:08 AM
Hello everyone,
I am an engineer at an EMS, and one of our clients has reported an issue related to the use of the HTS221TR sensor. Our client has observed that some of their boards, on which this sensor is mounted, have been exposed to projections of a product (specifically, wine) during their usage, resulting in inaccurate measurements.
Our boards are coated to prevent any degradation during their use, with the exception of the HTS221TR sensor.
I would like to seek your expertise on two points:
Best regards,
Axel
Solved! Go to Solution.
2023-12-01 12:57 AM
Hi @AxelH ,
Welcome to ST Community!
HTS221TR is not waterproof. There are micro-holes on the surface to read moisture, if liquid substances get inside we can no longer guarantee its function.
2023-12-01 12:57 AM
Hi @AxelH ,
Welcome to ST Community!
HTS221TR is not waterproof. There are micro-holes on the surface to read moisture, if liquid substances get inside we can no longer guarantee its function.
2023-12-01 1:30 AM
Hi Federica,
Thank you for your response.
I suspected this answer to some extent, but I still held a small hope for the possibility of cleaning.
I will inform the client about this matter.
Have a good day!