2022-05-25 9:49 AM
Hi!
I've configured an ISM330DHCX in CubeIDE with the X-CUBE-MEMS package. The code was generated, however, I have absolutely no idea how to initialize and use the sensor in my main.c code. So far I've managed to make following observations:
So how do I initialize the MEMS for 4-wire SPI bus, and why isn't this done automatically, when CubeMX even asks the user to point it to SPI instance responsible for communicationg with the sensor, as well as the CS pin for this task?
Thanks!
EDIT:
So far I've tried to use the library in the following way:
#include "custom_mems_conf.h"
#include "ism330dhcx.h"
static int32_t platform_write(void *handle, uint8_t reg, const uint8_t *bufp,
uint16_t len)
{
reg |= 0x40;
HAL_GPIO_WritePin(CUSTOM_ISM330DHCX_0_CS_PORT, CUSTOM_ISM330DHCX_0_CS_PIN, GPIO_PIN_RESET);
CUSTOM_ISM330DHCX_0_SPI_Send(®, 1);
CUSTOM_ISM330DHCX_0_SPI_Send((uint8_t*) bufp, len);
HAL_GPIO_WritePin(CUSTOM_ISM330DHCX_0_CS_PORT, CUSTOM_ISM330DHCX_0_CS_PIN, GPIO_PIN_SET);
return 0;
}
/*
* @brief Read generic device register (platform dependent)
*
* @param handle customizable argument. In this examples is used in
* order to select the correct sensor bus handler.
* @param reg register to read
* @param bufp pointer to buffer that store the data read
* @param len number of consecutive register to read
*
*/
static int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp,
uint16_t len)
{
reg |= 0xC0;
HAL_GPIO_WritePin(CUSTOM_ISM330DHCX_0_CS_PORT, CUSTOM_ISM330DHCX_0_CS_PIN, GPIO_PIN_RESET);
CUSTOM_ISM330DHCX_0_SPI_Send(®, 1);
CUSTOM_ISM330DHCX_0_SPI_Recv(bufp, len);
HAL_GPIO_WritePin(CUSTOM_ISM330DHCX_0_CS_PORT, CUSTOM_ISM330DHCX_0_CS_PIN, GPIO_PIN_SET);
return 0;
}
ISM330DHCX_IO_t io_ctx;
ISM330DHCX_Object_t ISM330;
ISM330DHCX_Axes_t axes_data;
uint8_t ISM_ID;
io_ctx.BusType = ISM330DHCX_SPI_4WIRES_BUS;
io_ctx.Init = BSP_SPI2_Init;
io_ctx.DeInit = BSP_SPI2_DeInit;
io_ctx.ReadReg = platform_read;
io_ctx.WriteReg = platform_write;
io_ctx.GetTick = HAL_GetTick;
ISM330DHCX_RegisterBusIO(&ISM330, &io_ctx);
ISM330DHCX_Init(&ISM330);
ISM330DHCX_ACC_Enable(&ISM330);
ISM330DHCX_ReadID(&ISM330, &ISM_ID);
ISM330DHCX_ACC_GetAxes(&ISM330, &axes_data);
But that's a blind shot, and I keep getting zeros everywhere (all axes, as well as ID are read as 0)
2022-06-15 9:38 AM
Hello @PSław.1,
Please, make sure to select ISM330DHCX Board Part as SPI, MOTION_SENSOR in the Board Support Custom in the X-CUBE-MEMS1 pack of CubeIDE and enable the correct pins for SPI and Chip Select. Make also sure that the Chip Select pin is initialized HIGH in the "System Core/GPIO" tab and that you select also a suitable SPI speed and mode (the sensor should support CPOL=0 and CPHASE=1Edge). At this point you can try to generate the code and in the main.c you can call:
CUSTOM_MOTION_SENSOR_Init(CUSTOM_ISM330DHCX_0, MOTION_ACCELERO|MOTION_GYRO);
to initialize the sensor and in the while(1) loop you can call:
CUSTOM_MOTION_SENSOR_Axes_t acc_value;
CUSTOM_MOTION_SENSOR_Axes_t gyr_value;
CUSTOM_MOTION_SENSOR_GetAxes(CUSTOM_ISM330DHCX_0, MOTION_ACCELERO, &acc_value);
CUSTOM_MOTION_SENSOR_GetAxes(CUSTOM_ISM330DHCX_0, MOTION_GYRO, &gyr_value);
to get the values of accelerometer and gyroscope.
Best Regards,
Carlo
2025-01-23 9:16 PM
Hi
"I am using the STM32F407 to interface with the ISM330DHCX. I have installed the X-CUBE MEMS1 package, configured the SPI1 protocol, and generated the code. How should I write the code correctly?" Let me know some suggestions.