cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a Linux driver for iis2dlpctr available? Or is there an update of st_accel_i2c.c with iis2dlpctr? Or include st_accel_i2c.c an compatible type ? What i must include for iis2dlpctr into the dtb file ".compatible = "st,...",

KScha.3
Associate II
 
2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @KScha.3​ ,

I suggest you to rise a question directly on ST Linux driver page for MEMS&Sensors on Github:

GitHub - STMicroelectronics/STMems_Linux_Input_drivers: This repository contains Linux kernel (v3.10, v3.4) with STMicroelectronics MEMS Input sensor support

This will allow ST Linux experts to answer directly to the question.

-Eleon

KScha.3
Associate II

Hi. Thanks for your help but unfortunately I can't find a driver with the name iis2dlpctr or what is the name/path of the driver that I can use for this sensor. Thanks