‎2021-02-24 03:40 AM
Hi everyone, I'm using an STM32L4 microcontroller and a LSM6DSL MEMS. They are conected with the spi2 interface and for configuring everithing I'm using STMCubeIDE.
I'm able to use the MEMS without BSP Custom, but when I try to set the BSP, it doesn't work at all.
Here the code I used to link BSP with SPI:
/* Link SPI functions to the LSM6DSL driver */
io_ctx.BusType = LSM6DSL_SPI_4WIRES_BUS;
io_ctx.Init = BSP_SPI2_Init;
io_ctx.DeInit = BSP_SPI2_DeInit;
io_ctx.ReadReg = BSP_SPI2_SendRecv;
io_ctx.WriteReg = BSP_SPI2_Send;
io_ctx.GetTick = BSP_GetTick;
LSM6DSL_RegisterBusIO(&MotionSensor, &io_ctx);
I have read on internet that it works fine with I2C, but it seems to be a little tricky to set it up with SPI.
Anyone could help?
Thanks
Gabriele
Solved! Go to Solution.
‎2021-02-25 12:38 AM
Hello everyone again,
I solved the issue. My mistake was in these two line:
io_ctx.ReadReg = BSP_SPI2_SendRecv;
io_ctx.WriteReg = BSP_SPI2_Send;
BSP_SPI2_SendRecv and BSP_SPI2_Send functions are incompatible so I did the following wrap:
int32_t wrap_platform_read(uint8_t Address, uint8_t Reg, uint8_t *Bufp, uint16_t len){
Reg |= 0x80;
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_RESET);
BSP_SPI2_Send(&Reg, 1);
BSP_SPI2_SendRecv(&Reg, Bufp, len);
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_SET);
return P_OK;
}
int32_t wrap_platform_write(uint8_t Address, uint8_t Reg, uint8_t *Bufp, uint16_t len){
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_RESET);
BSP_SPI2_Send(&Reg, 1);
BSP_SPI2_Send(Bufp, len);
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_SET);
return P_OK;
}
and here the correct link:
/* Link SPI functions to the LSM6DSL driver */
io_ctx.BusType = LSM6DSL_SPI_4WIRES_BUS;
io_ctx.Address = 0;
io_ctx.Init = BSP_SPI2_Init;
io_ctx.DeInit = BSP_SPI2_DeInit;
io_ctx.ReadReg = platform_read;
io_ctx.WriteReg = platform_write;
io_ctx.GetTick = BSP_GetTick;
LSM6DSL_RegisterBusIO(&MotionSensor, &io_ctx);
:grinning_face:
‎2021-02-25 12:38 AM
Hello everyone again,
I solved the issue. My mistake was in these two line:
io_ctx.ReadReg = BSP_SPI2_SendRecv;
io_ctx.WriteReg = BSP_SPI2_Send;
BSP_SPI2_SendRecv and BSP_SPI2_Send functions are incompatible so I did the following wrap:
int32_t wrap_platform_read(uint8_t Address, uint8_t Reg, uint8_t *Bufp, uint16_t len){
Reg |= 0x80;
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_RESET);
BSP_SPI2_Send(&Reg, 1);
BSP_SPI2_SendRecv(&Reg, Bufp, len);
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_SET);
return P_OK;
}
int32_t wrap_platform_write(uint8_t Address, uint8_t Reg, uint8_t *Bufp, uint16_t len){
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_RESET);
BSP_SPI2_Send(&Reg, 1);
BSP_SPI2_Send(Bufp, len);
HAL_GPIO_WritePin(CS_SPI2_GPIO_Port, CS_SPI2_Pin, GPIO_PIN_SET);
return P_OK;
}
and here the correct link:
/* Link SPI functions to the LSM6DSL driver */
io_ctx.BusType = LSM6DSL_SPI_4WIRES_BUS;
io_ctx.Address = 0;
io_ctx.Init = BSP_SPI2_Init;
io_ctx.DeInit = BSP_SPI2_DeInit;
io_ctx.ReadReg = platform_read;
io_ctx.WriteReg = platform_write;
io_ctx.GetTick = BSP_GetTick;
LSM6DSL_RegisterBusIO(&MotionSensor, &io_ctx);
:grinning_face:
‎2021-02-25 02:35 AM
Good job Gabriele! :smiling_face_with_smiling_eyes:
And thank you very much for reporting your solution
-Eleon