cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to work with the STEVAL-MKI142V1 without STEVAL-MKI109V2 ?

David DIMANCHE
Associate
Posted on July 11, 2017 at 12:48

Hi,

I am trying to test my I2C connection with my STM32nucleoF411RE but I can't seems to have any response from my MKI142V1. I have tested the start condition and sending the address but it doesn't seem to retrieve the acknowledge bit that the sensor should send back. 

So my question is, can I really test the MKI142V1 without MKI109V2 that everyone recommends ?

1 REPLY 1
Miroslav BATEK
ST Employee
Posted on July 11, 2017 at 13:41

Yes, you can. The STEVAL-MKI142V1 is just a adapter board, you can check the schematic

http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-tools/mems-motion-sensor-eval-boards/steval-mki142v1.html

.

Don't forget to connect Vdd and Vdd_IO to power supply and the CS to Vdd to enable I2C.