2021-03-03 08:24 AM
Solved! Go to Solution.
2021-03-03 09:15 AM
yes, it is. In the webinar an example has been provided: the recording of a moderate earthquake (ML 3.9) which happened in Milan while the IIS2ICLX was under long term testing. In general, IIS2ICLX has a noise density extremely low (so a very high resolution) and the capability of recording acceleration up to 260Hz with great resolution
2021-03-03 09:15 AM
yes, it is. In the webinar an example has been provided: the recording of a moderate earthquake (ML 3.9) which happened in Milan while the IIS2ICLX was under long term testing. In general, IIS2ICLX has a noise density extremely low (so a very high resolution) and the capability of recording acceleration up to 260Hz with great resolution