2020-02-10 4:58 AM
In my STM32 Discovery L4 board I have inertial MEMS sensors L3GD20 gyroscope and LSM303C e-compass (accelerometer+magnotemeter), all of them with different Output Data Rate, by default in BSP 95 Hz, 50 Hz, 40 Hz respectively.
In order to make a sensor fusion, how must to adjust a periodic timer to take correct samples?
Thanks in advance.
2020-02-26 2:48 AM
Hi @josan , the ideal would be to have same ODR among sensors or at least a common multiple ODR. However, please consider this statement of the standard MotionFX library for the sensor fusion (NUCLEO environment):
100 Hz is recommended. The output data rate for:
I suggest you to acquire the data at the maximum ODR (e.g. 95 Hz) and manage the duplicated values of the other sensor acquisitions discarding them during the data processing.
Regards