2019-04-25 11:05 AM
Dear Community,
I am excited to get started with the IIS3DHHC sensor in combination with an Arduino Teensy. I have been working before with the Analog Devices ADXL355, I've successfully wrote a program for this, but I have difficulties knowing if I'm going into the right direction with the IIS3DHHC.
Would anyone be able to give me a bit of guidance on my code and say if I'm going into the right direction?
Many thanks,
Chris
2019-04-30 07:13 AM
hi Chris
Btw, could you share me the oscilloscope or logic analyzer pattern? Did you receive the ack from the slave? At which Vdd/VddIO are you working?
Regards