2022-06-06 9:00 AM
But when I add calling a fall algorithm task after reading each sample and try to simulate a fall (the rapid moment) causing program not causing interrupt.
Any help regarding why interrupt is not set would be of great help.
//code
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t status;
uint16_t watermark;
uint8_t tag;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Config code for STM32_WPAN (HSE Tuning must be done before system clock configuration) */
MX_APPE_Config();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* IPCC initialisation */
MX_IPCC_Init();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_RF_Init();
MX_RTC_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Init code for STM32_WPAN */
MX_APPE_Init();
/* Infinite loop */
/* USER CODE BEGIN WHILE */
/* Initializing the LSM6DSOX sensor */
MY_MOTION_SENSOR_CUSTOM();
/* Register my_task to sequencer */
UTIL_SEQ_RegTask(1 << CFG_TASK_MY_TASK_ID, UTIL_SEQ_RFU, my_task);
status = 1;
watermark = 10;
CUSTOM_MOTION_SENSOR_FIFO_Set_Watermark_Level(CUSTOM_LSM6DSOX_0, watermark);
uint8_t regVal = 0;
CUSTOM_MOTION_SENSOR_FIFO_Set_Mode(CUSTOM_LSM6DSOX_0, LSM6DSOX_BYPASS_MODE);
CUSTOM_MOTION_SENSOR_Write_Register(CUSTOM_LSM6DSOX_0, LSM6DSOX_FIFO_CTRL3, 0x44);
CUSTOM_MOTION_SENSOR_FIFO_Set_Mode(CUSTOM_LSM6DSOX_0, LSM6DSOX_STREAM_MODE);
CUSTOM_MOTION_SENSOR_FIFO_Set_INT2_FIFO_Watermark(CUSTOM_LSM6DSOX_0, status);
uint8_t buff[6];
axis3bit16_t data_raw_acceleration;
float acceleration_mg[3];
while (1)
{
//Declaring local variables
uint8_t wmflag = 0;
uint16_t numberSamples = 0;
axis3bit16_t dummy;
CUSTOM_MOTION_SENSOR_FIFO_Get_WMFlag(CUSTOM_LSM6DSOX_0, &wmflag);
if (Get_Read_Flag()) {
Set_Read_Flag(0);
numberSamples = 0;
/* Read Number Samples */
CUSTOM_MOTION_SENSOR_FIFO_Get_Num_Samples(CUSTOM_LSM6DSOX_0, &numberSamples);
snprintf(dataOut, MAX_BUF_SIZE, "BEG Num Samples %d\r\n", numberSamples);
printf("%s", dataOut);
while (numberSamples--)
{
CUSTOM_MOTION_SENSOR_FIFO_Get_Tag(CUSTOM_LSM6DSOX_0, &tag);
switch (tag) {
case LSM6DSOX_XL_NC_TAG:
memset(data_raw_acceleration.u8bit, 0x00, 3 * sizeof(int16_t));
CUSTOM_MOTION_SENSOR_Read_raw_FIFO_data(CUSTOM_LSM6DSOX_0, data_raw_acceleration.u8bit);
// call fall detection algorithm here
fall_detection();
break;
default:
/* Flush unused samples */
memset(dummy.u8bit, 0x00, 3 * sizeof(int16_t));
CUSTOM_MOTION_SENSOR_Read_raw_FIFO_data(CUSTOM_LSM6DSOX_0, dummy.u8bit);
break;
}
}
}
HAL_Delay(400);
}
while(1)
/* USER CODE END WHILE */
{
MX_APPE_Process();
/* USER CODE BEGIN 3 */
UTIL_SEQ_SetTask(1 << CFG_TASK_MY_TASK_ID, CFG_SCH_PRIO_0);
}
}
// Code to set interrupt
/**
* @brief Set the LSM6DSOX FIFO watermark on INT2 pin
* @param pObj the device pObj
* @param Status FIFO watermark interrupt on INT2 pin status
* @retval 0 in case of success, an error code otherwise
*/
int32_t LSM6DSOX_FIFO_Set_INT2_FIFO_Watermark(LSM6DSOX_Object_t *pObj, uint8_t Status)
{
// lsm6dsox_reg_t reg;
lsm6dsox_int2_ctrl_t reg;
// if (lsm6dsox_read_reg(&(pObj->Ctx), LSM6DSOX_INT2_CTRL, ®.byte, 1) != LSM6DSOX_OK)
if (lsm6dsox_read_reg(&(pObj->Ctx), LSM6DSOX_INT2_CTRL, (uint8_t*)®, 1) != LSM6DSOX_OK)
{
return LSM6DSOX_ERROR;
}
reg.int2_fifo_th = 1;
if (lsm6dsox_write_reg(&(pObj->Ctx), LSM6DSOX_INT2_CTRL, (uint8_t*)®, 1) != LSM6DSOX_OK)
{
return LSM6DSOX_ERROR;
}
return LSM6DSOX_OK;
}
// External interrupt callback.
/* USER CODE BEGIN FD_WRAP_FUNCTIONS */
void HAL_GPIO_EXTI_Callback( uint16_t GPIO_Pin )
{
//printf("GPIO_Pin %d\n\r",GPIO_Pin);
switch (GPIO_Pin)
{
case BUTTON_SW1_PIN:
APP_BLE_Key_Button1_Action();
break;
case BUTTON_SW2_PIN:
APP_BLE_Key_Button2_Action();
break;
case BUTTON_SW3_PIN:
APP_BLE_Key_Button3_Action();
break;
default:
break;
}
if (GPIO_Pin == 64) {
readFlag = 1;
}
return;
}
2022-06-06 3:53 PM
@vtall.1 "LSMDSOX sensor"
Do you mean LSM6DSOX ?
"try to simulate a fall (the rapid moment) causing program not causing interrupt."
Do you mean the accelerometer doesn't generate an interrupt, or the STM32 doesn't see the interrupt?