2022-11-10 10:08 PM
I have recently brought a STEVAL-STLKT01V1 SensorTile kit in which LSM6DSM, LSM303AGR & LPS22HB are connected in 3 wire SPI on the SPI2 line of STM32L476. I pulled 4 CS lines to high at the beginning of the program and have set the SPI2 to Half duplex master mode with low data transfer rate. even though using the c command lsm6dsm_spi_mode_set(&dev_ctx, LSM6DSM_AUX_SPI_3_WIRE); I'm getting no response on spi read, so the program is getting struck at lsm6dsm_reset_get(&dev_ctx, &rst).
I was able to use 4 wire SPI with STM32F407 and LSM6DSM, but I still face issues with using 3 Wire mode with STM32F407 and LSM6DSM
i have defined the CS Pin:
#define CS_up_GPIO_Port CS_AG_GPIO_Port
#define CS_up_Pin CS_AG_Pin
my GPIO Configuration:
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOG_CLK_ENABLE();
HAL_PWREx_EnableVddIO2();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(BLUE_RST_GPIO_Port, BLUE_RST_Pin, GPIO_PIN_SET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, CS_AG_Pin|BLUE_CS_Pin|CS_M_Pin, GPIO_PIN_SET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(CS_P_GPIO_Port, CS_P_Pin, GPIO_PIN_SET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(CS_A_GPIO_Port, CS_A_Pin, GPIO_PIN_SET);
/*Configure GPIO pin : LED_Pin */
GPIO_InitStruct.Pin = LED_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : BLUE_RST_Pin */
GPIO_InitStruct.Pin = BLUE_RST_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(BLUE_RST_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : CS_AG_Pin BLUE_CS_Pin CS_M_Pin */
GPIO_InitStruct.Pin = CS_AG_Pin|BLUE_CS_Pin|CS_M_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*Configure GPIO pin : CS_P_Pin */
GPIO_InitStruct.Pin = CS_P_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(CS_P_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : CS_A_Pin */
GPIO_InitStruct.Pin = CS_A_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(CS_A_GPIO_Port, &GPIO_InitStruct);
}
my SPI Mode Configuration:
static void MX_SPI2_Init(void)
{
/* USER CODE BEGIN SPI2_Init 0 */
/* USER CODE END SPI2_Init 0 */
/* USER CODE BEGIN SPI2_Init 1 */
/* USER CODE END SPI2_Init 1 */
/* SPI2 parameter configuration*/
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_1LINE;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI2_Init 2 */
/* USER CODE END SPI2_Init 2 */
}
Sensor Initialization:
/* Initialize mems driver interface */
stmdev_ctx_t dev_ctx;
dev_ctx.write_reg = platform_write;
dev_ctx.read_reg = platform_read;
dev_ctx.handle = &SENSOR_BUS;
/* Wait sensor boot time */
HAL_Delay(15);
lsm6dsm_spi_mode_set(&dev_ctx, LSM6DSM_AUX_SPI_3_WIRE);
lsm6dsm_auto_increment_set(&dev_ctx, 1);
/* Restore default configuration */
lsm6dsm_reset_set(&dev_ctx, PROPERTY_ENABLE);
do {
lsm6dsm_reset_get(&dev_ctx, &rst);
} while (rst);
/* Enable Block Data Update */
lsm6dsm_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/* Set Output Data Rate for Acc and Gyro */
lsm6dsm_xl_data_rate_set(&dev_ctx, LSM6DSM_XL_ODR_12Hz5);
lsm6dsm_gy_data_rate_set(&dev_ctx, LSM6DSM_GY_ODR_12Hz5);
/* Set full scale */
lsm6dsm_xl_full_scale_set(&dev_ctx, LSM6DSM_2g);
lsm6dsm_gy_full_scale_set(&dev_ctx, LSM6DSM_2000dps);
/* Configure filtering chain(No aux interface)
* Accelerometer - analog filter
*/
lsm6dsm_xl_filter_analog_set(&dev_ctx, LSM6DSM_XL_ANA_BW_400Hz);
/* Accelerometer - LPF1 path (LPF2 not used) */
//lsm6dsm_xl_lp1_bandwidth_set(&dev_ctx, LSM6DSM_XL_LP1_ODR_DIV_4);
/* Accelerometer - LPF1 + LPF2 path */
lsm6dsm_xl_lp2_bandwidth_set(&dev_ctx, LSM6DSM_XL_LOW_NOISE_LP_ODR_DIV_100);
/* Accelerometer - High Pass / Slope path */
//lsm6dsm_xl_reference_mode_set(&dev_ctx, PROPERTY_DISABLE);
//lsm6dsm_xl_hp_bandwidth_set(&dev_ctx, LSM6DSM_XL_HP_ODR_DIV_100);
/* Gyroscope - filtering chain */
lsm6dsm_gy_band_pass_set(&dev_ctx, LSM6DSM_HP_260mHz_LP1_STRONG);
SPI Read & Write:
static int32_t platform_write(void *handle, uint8_t reg,
uint8_t *bufp,
uint16_t len)
{
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(handle, ®, 1, 1000);
HAL_SPI_Transmit(handle, bufp, len, 1000);
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_SET);
}
static int32_t platform_read(void *handle, uint8_t reg, uint8_t *bufp,
uint16_t len)
{
reg |= 0x80;
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(handle, ®, 1, 1000);
HAL_SPI_Receive(handle, bufp, len, 1000);
HAL_GPIO_WritePin(CS_up_GPIO_Port, CS_up_Pin, GPIO_PIN_SET);
}
kindly reply what's the issue with the above-followed procedure
2022-12-26 09:13 PM
Hi @Soundhar . Can you solved the problem ?
2024-10-07 06:47 AM
Hi,
Can you solved the problem? Because I have know the same problem.