2019-02-04 5:22 AM
Hi, I am using STPM33 for energy monitering. I have 2 STPM33 in my design and hence there are 4 current sense channels where I use shunt resistors for sensing. The problem faced by me is that the fourth channel is showing an offset of 6 mA when zero current is flowing through the shunt. I was able to reduce it by reducing the low pass filter resistor between the stpm33 and shunt resistor from 1K to 220Ohm. Still the 4th channel has got 3mA offset where as all other ports show 1-2mA for zero current through their respective sense resistors. Anyway 3mA is acceptable for me but I want to know why this happens and if there is a better way to solve this problem. aAlso I want to know the significance of 1k resistor as low pass filter. Somebody please help.
2019-02-05 9:05 AM
hi, STPM33 is not a MEMS sensor.
You should forward your question to power and motor control section https://community.st.com/s/topic/0TO0X000000BSqZWAW/power-management-and-motor-control