2019-09-14 9:55 PM
Hi
Is there a way to perform a factory reset for SensorTile? For some reason, my laptop can't detect it anymore. Device manager said "This device cannot start. (Code 10). A device which does not exist was specified." I try to erase full chip flash memory and plan to load the original bootloader, but I also get error message in CubeProgrammer
"Error: Invalid port name: No DFU detEstablishing connection with the device failed"
Pressing the root button doesn't seem to help. I first tried to press the button after connecting to a laptop, but it didn't help. I also tried to hold the root button and release it after connecting to the laptop, but it also didn't help.
May I know what I am missing?
Thanks,
Dennis
2019-11-24 5:50 PM
Got it, thanks. Will email you privately. Thanks!
2020-02-17 4:22 AM
Can you also do that for me?