cancel
Showing results for 
Search instead for 
Did you mean: 

How do I have to use "VL53L4CD_Start_Temperature_Update()’ function to compensate temperature drift?

OLope.11
Associate

I have measured an offset drift around 6 mm when I heat VL53L4CD sensor from 24ºC to 45ºC. In order to reduce this error, I used "VL53L4CD_Start_Temperature_Update()’ once ranging was stopped. Unfortunately, it has no effect on the measurements and I observed that a timeout error was obtained from this function. Please, may anyone provide me any example where this function is applied properly. 

0 REPLIES 0