cancel
Showing results for 
Search instead for 
Did you mean: 

How do I download an older version of X-CUBE-MEMS1 (V4.4.1) since I am running an older A1 version sensor board

Bill Dempsey
Senior

Latest (6.x) release does not support my existing boards and I need to keep these running.

3 REPLIES 3
Eleon BORLINI
ST Employee

Hi Bill, you can download X-CUBE-MEMS1 (V4.4.1) at this link:

https://www.st.com/en/embedded-software/x-cube-mems1-v4.html

HOwever, I suggest you to upgrade the X-NUCLEO-IKS01A1 to the last X-NUCLEO-IKS01A3 which includes the interface for the last ST sensors

Regards

Bill Dempsey
Senior

Hi, Thank you! I will download these.

I did try to order the A3 but it is not ready for sale. I ordered the A2 and it works.

Regards

Bill

Eleon BORLINI
ST Employee

yes, it will be available soon!

regards​