Skip to main content
DPark.4
Associate
September 16, 2020
Question

How can I get the dimension of STEVAL-MKI208V1K?

  • September 16, 2020
  • 10 replies
  • 5566 views

..

    This topic has been closed for replies.

    10 replies

    Eleon BORLINI
    ST Employee
    September 16, 2020

    Hi @DPark.4​ ,

    the X-Y dimensions of the industrial adapter STEVAL-MKI208V1K are 2.45x2.45cm.

    You can check it by opening the gerber files available on the site under the Hardware Resources section, STEVAL-MKI208V1K GERBER.

    You can open the files with your pcb design software or otherwise with a free online gerber viewer allowing planar measures.

    -Eleon

    DPark.4
    DPark.4Author
    Associate
    September 16, 2020

    Thank you for your reply. I opened the Gerber file through online Gerber viewer but I cannot check the size like hole size, hole position, and so on. Could you help me to have the dimension or 3D file?

    Eleon BORLINI
    ST Employee
    September 17, 2020

    Hi @DPark.4​ ,

    please find the 3D pdf file for the dimensional measures below in attachment.

    Please let me know if it is ok.

    -Eleon

    Federica Bossi
    ST Technical Moderator
    September 21, 2023

    Hi @kubark42 ,

    I really don't understand the reason why the boards you mention have not same size we have discussed

     

    Our normal plan is to do the same size for square boards and the size center hole to center hole is 20.4mm in both X and Y coordinates.
    Concerning the size of the board, this is 25mm*25mm (+/-0.5mm depending the drilling machine). The size of the hole is 2mm as per STEVAL-MKI208V1 DRR file you find here:

    FedericaBossi_0-1695286061328.png

    3 mm is the metallization of the 2mm holes.

    If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Visitor II
    December 10, 2023

    Here is the drawing which should have been present in the original documentation, and, failing that, should have been uploaded by ST's forum employees. 

    Screenshot 2023-12-10 at 10.45.16 AM.png

    Note that the board outer tolerance is given as +0/-0.5, taking into account a previous statement that it's categorically 24.5mm, but then later on a pseudo-correction that it could be 25+-0.5. I'm doing my best to merge those two somewhat contradictory statements.

    =============================================

    A general plea to ST: please don't make your clients do this work for you. This is a somewhat pricey board, it should come with the support required to mount it. It should not take knowledge of how ST does other square boards, nor software for opening gerbers and drill files.