cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSL partially failling self-tests

SMari.10
Associate II

Hello everyone,

 

I am currently trying to use a LSM6DSL (accelerometer and gyroscope) but only the accelerometer works.

 

I am using a NUCLEO-L476RG with a LSM6DSL from a STEVAL-MKI178V2 with the st library : lsm6dsl.c/h and lsm6dsl_reg.c/h

After the init I get the correct values from the acc but not from the gyro (out of scale values when I am expecting close to 0).

So I have implemented the self tests given int he application notes (attached file) p.96-99.

 

The accelerometer passes its test but not the gyroscope, which have deltas over 300K dps.

 

Here is my gyro's self-test :

 

bool pSensorTask_GYRO_SelfTest(void){
  bool status = false;
  LSM6DSL_Axes_t axes_delta = {0};
  LSM6DSL_Axes_t axes_withoutSelf = {0};
  LSM6DSL_Axes_t axes_withSelf = {0};
  LSM6DSL_AxesRaw_t axes_raw = {0};
  LSM6DSL_Axes_t mAxesRaw_withoutSelf = {0};
  LSM6DSL_Axes_t mAxesRaw_withSelf = {0};
  float sensitivity;
  uint8_t nb_data = 0;
  uint8_t drdy = 0;

  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL1_XL, 0x00);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL2_G, 0x5c);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL3_C, 0x44);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL4_C, 0x00);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL5_C, 0x00);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL6_C, 0x00);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL7_G, 0x00);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL8_XL, 0x00);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL9_XL, 0x00);
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL10_C, 0x00);
  HAL_Delay(150);

  do{
    LSM6DSL_GYRO_Get_DRDY_Status(&MotionSensor, &drdy);
    HAL_Delay(1);
  }while(drdy != true);

  LSM6DSL_GYRO_GetAxesRaw(&MotionSensor, &axes_raw);         /* Clear DRDY */

  for(nb_data = 0; nb_data < 5; nb_data++)
  {
    do{
      LSM6DSL_GYRO_Get_DRDY_Status(&MotionSensor, &drdy);
      HAL_Delay(1);
    }while(drdy != true);

    LSM6DSL_GYRO_GetAxesRaw(&MotionSensor, &axes_raw);
    mAxesRaw_withoutSelf.x += axes_raw.x;
    mAxesRaw_withoutSelf.y += axes_raw.y;
    mAxesRaw_withoutSelf.z += axes_raw.z;
  }

  mAxesRaw_withoutSelf.x /= 5;
  mAxesRaw_withoutSelf.y /= 5;
  mAxesRaw_withoutSelf.z /= 5;

  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL5_C, 0x04);
  HAL_Delay(50);

  do{
    LSM6DSL_GYRO_Get_DRDY_Status(&MotionSensor, &drdy);
    HAL_Delay(1);
  }while(drdy != true);

  LSM6DSL_GYRO_GetAxesRaw(&MotionSensor, &axes_raw);         /* Clear DRDY */

  for(nb_data = 0; nb_data < 5; nb_data++)
  {
    do{
      LSM6DSL_GYRO_Get_DRDY_Status(&MotionSensor, &drdy);
      HAL_Delay(1);
    }while(drdy != true);

    LSM6DSL_GYRO_GetAxesRaw(&MotionSensor, &axes_raw);
    mAxesRaw_withSelf.x += axes_raw.x;
    mAxesRaw_withSelf.y += axes_raw.y;
    mAxesRaw_withSelf.z += axes_raw.z;
  }

  mAxesRaw_withSelf.x /= 5;
  mAxesRaw_withSelf.y /= 5;
  mAxesRaw_withSelf.z /= 5;

  LSM6DSL_GYRO_GetSensitivity(&MotionSensor, &sensitivity);
  axes_withoutSelf.x = (int32_t)((float)((float)mAxesRaw_withoutSelf.x * sensitivity));
  axes_withoutSelf.y = (int32_t)((float)((float)mAxesRaw_withoutSelf.y * sensitivity));
  axes_withoutSelf.z = (int32_t)((float)((float)mAxesRaw_withoutSelf.z * sensitivity));

  axes_withSelf.x = (int32_t)((float)((float)mAxesRaw_withSelf.x * sensitivity));
  axes_withSelf.y = (int32_t)((float)((float)mAxesRaw_withSelf.y * sensitivity));
  axes_withSelf.z = (int32_t)((float)((float)mAxesRaw_withSelf.z * sensitivity));

  axes_delta.x = axes_withSelf.x - axes_withoutSelf.x;
  axes_delta.y = axes_withSelf.y - axes_withoutSelf.y;
  axes_delta.z = axes_withSelf.z - axes_withoutSelf.z;

  if((abs(axes_delta.x) >= 150) && (abs(axes_delta.x) <= 700) && \
    (abs(axes_delta.y) >= 150) && (abs(axes_delta.y) <= 700) && \
  (abs(axes_delta.z) >= 150) && (abs(axes_delta.z) <= 700))
  {
    status = true;
  }

  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL2_G, 0x00); /* Disable Sensor */
  LSM6DSL_Write_Reg(&MotionSensor, LSM6DSL_CTRL5_C, 0x00); /* Disable self test */

  return status;

}

 

 

I seriously doubt that the hardware is the issue as the acc is perfectly fine.

 

Can anyone help me ?

 

Don't hesitate to ask me if I have forgot any information.

 

Thanks in advance.

 

Regards,

 

MARIE

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
SMari.10
Associate II

Hi !

I have found the solution.

I had misinterpreted the lsm6 documentation (attached file).

At page 22, the min/max values of the accelerometer are in mg while the gyroscope's one are in dps :

SMari10_0-1702289486134.png

But the returned value from the gyro are in mdps, not dps !

SMari10_1-1702289563601.png

So the comparison of the deltas must be in mdps : 150,000 < deltas < 700,000.

I fixed it in my code and it's now working !

View solution in original post

1 REPLY 1
SMari.10
Associate II

Hi !

I have found the solution.

I had misinterpreted the lsm6 documentation (attached file).

At page 22, the min/max values of the accelerometer are in mg while the gyroscope's one are in dps :

SMari10_0-1702289486134.png

But the returned value from the gyro are in mdps, not dps !

SMari10_1-1702289563601.png

So the comparison of the deltas must be in mdps : 150,000 < deltas < 700,000.

I fixed it in my code and it's now working !