2023-06-29 6:25 AM
I would like to calibrate 2 magnetic sensors concurrently with MotionMC library. However, the functions from the library for MotionMC_Initialize, MotionMC_Update and MotionMC_GetCalParams do not need inputting an ID. If calibrate 2 sensors in the same time or power cycle, whether will HI_Bias[3] and SF_Matrix[3][3] coefficients be overwritten?
I do appreciate any idea for calibrating 2 magnetic sensors in same time with MotionMC library.
Qingshan
2023-07-11 4:54 AM
Hi @QShan.1 ,
what you want to do is feasible, you have to write a function to which you feed also the sensor ID, that keeps track of the 2 different HI_Bias[3] and SF_Matrix[3][3] for the different sensors.
if you managed to perform the calibration of one sensor, this would be quite easy =)
If this answers your question, please, mark this as "best answer", by clicking on the "accept as solution" to help the other users of the community
Niccolò