2021-02-23 9:31 PM
can u help me fix this issue? sometime it gives alert when there is no noise
Solved! Go to Solution.
2021-02-24 5:05 AM
Hi @ShivaRagu ,
Did you installed the last firmware on the board (the smartphone and). You have then to enable the Bluetooth and the localization service on your smartphone.
You are then able to upload the Baby crying app, that has a dedicated "homepage" and should activate the green LED on the board when a baby cry is detected.
If you have done all these steps without success, I suggest you to try with the attached bin firmware version and upload it on the sensortile.box board as described in this post.
Please let me know in case of any progress.
-Eleon
2021-02-24 5:05 AM
Hi @ShivaRagu ,
Did you installed the last firmware on the board (the smartphone and). You have then to enable the Bluetooth and the localization service on your smartphone.
You are then able to upload the Baby crying app, that has a dedicated "homepage" and should activate the green LED on the board when a baby cry is detected.
If you have done all these steps without success, I suggest you to try with the attached bin firmware version and upload it on the sensortile.box board as described in this post.
Please let me know in case of any progress.
-Eleon
2021-02-24 8:17 PM
hi thanks a lot for your answer.
2021-02-25 11:15 PM
Hi,
I have updated the firmware in both Smartphone & Device. Still the baby crying detector is getting triggered when there in no noise.
The Green LED started to blink without the noise.
Please help me to fix this.
2021-02-26 12:24 AM
Hi @ShivaRagu ,
that's strange... are you using the last firmware I shared above?
I suggest you to re-load the "Baby Crying detector" app, and if it still doesn't work please disconnect and reconnect the battery.
-Eleon
2021-02-26 12:53 AM
Hi,
Ok will try that & confirm you.
2022-05-13 10:47 PM
Baby Crying Detector App is very useful for Moms, Mom can take care his Children.
2022-10-12 1:32 AM
What firmware version of SensorTile.box did you test with? If you test with v3.4.9, most of the accelerometer demo apps and AI sound classification app will not work. Try downgrading to Sensortile.box firmware to version 3.4.7 and test it.
2022-11-04 9:11 AM
I have this v349 and literally none of the basic apps work when going the Create App play route. Only the original apps on connect work at all.
How can I get back to v347? Downgrade?
Using the iPhone BLE Sensor app BTW
2022-11-04 10:30 AM