Hi, I'm trying to program my STN32G431RB in order to work with the sensor HTS221, I write the code but I don't know if it's correct, I would be really grateful if someone could tell me.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-28 01:03 AM
while (1)
{
/* USER CODE END WHILE */
for (int i=0; i<11; i++)
{
buf1[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf1[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf2[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf3[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf4[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf5[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf6[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf7[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf8[i]=0x0;
}
for (int i=0; i<11; i++)
{
buf9[i]=0x0;
}
buf9[0] = WIA;
ret9 = HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf9, 1, HAL_MAX_DELAY);
if (ret9 != HAL_OK) {
strcpy((char*)buf9, "Error Tx\r\n");
} else{
ret9 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf9, 2, HAL_MAX_DELAY);
if (ret9 != HAL_OK ) {
strcpy((char*)buf9, "Error Rx\r\n");
}else {
}
}
//Lettura umiditÃ
buf1[0] = REGH_MSB;
ret1 = HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf1, 1, HAL_MAX_DELAY);
if (ret1 != HAL_OK) {
strcpy((char*)buf1, "Error Tx\r\n");
} else{
ret1 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf1, 2, HAL_MAX_DELAY);
if (ret1 != HAL_OK ) {
strcpy((char*)buf1, "Error Rx\r\n");
}else {
buf2[0] = REGH_LSB;
ret2 = HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf2, 1, HAL_MAX_DELAY);
if (ret2 != HAL_OK) {
strcpy((char*)buf2, "Error Tx\r\n");
} else{
ret2 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf2, 2, HAL_MAX_DELAY);
if (ret2 != HAL_OK ) {
strcpy((char*)buf2, "Error Rx\r\n");
}else {
H_OUT= buf1[0]<<8 | buf2[0];
}
}
}
}
//Lettura valori per conversione umiditÃ
//1-H0_T0_OUT
buf3[0] = REG_H0_T0_OUT_LSB ;
ret3= HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf3, 1, HAL_MAX_DELAY);
if (ret3 != HAL_OK) {
strcpy((char*)buf3, "Error Tx\r\n");
} else{
ret3 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf3, 2, HAL_MAX_DELAY);
if (ret1 != HAL_OK ) {
strcpy((char*)buf3, "Error Rx\r\n");
}else {
buf4[0] = REG_H0_T0_OUT_MSB;
ret4 = HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf4, 1, HAL_MAX_DELAY);
if (ret4 != HAL_OK) {
strcpy((char*)buf4, "Error Tx\r\n");
} else{
ret4 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf4, 2, HAL_MAX_DELAY);
if (ret4 != HAL_OK ) {
strcpy((char*)buf4, "Error Rx\r\n");
}else {
H0_T0_OUT= buf4[0]<<8 | buf3[0];
}
}
}
}
//2-H1_T0_OUT
buf5[0] = REG_H1_T0_OUT_LSB ;
ret5= HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf5, 1, HAL_MAX_DELAY);
if (ret5 != HAL_OK) {
strcpy((char*)buf5, "Error Tx\r\n");
} else{
ret5 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf5, 2, HAL_MAX_DELAY);
if (ret5 != HAL_OK ) {
strcpy((char*)buf5, "Error Rx\r\n");
}else {
buf6[0] = REG_H1_T0_OUT_MSB;
ret6 = HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf6, 1, HAL_MAX_DELAY);
if (ret6 != HAL_OK) {
strcpy((char*)buf6, "Error Tx\r\n");
} else {
ret6 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf6, 2, HAL_MAX_DELAY);
if (ret6 != HAL_OK ) {
strcpy((char*)buf6, "Error Rx\r\n");
}else {
H1_T0_OUT= buf6[0]<<8 | buf5[0];
}
}
}
}
//3-H0_rHx2
buf7[0] = REG_H0_rH;
ret7= HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf7, 1, HAL_MAX_DELAY);
if (ret7 != HAL_OK) {
strcpy((char*)buf7, "Error Tx\r\n");
} else{
ret7 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf7, 2, HAL_MAX_DELAY);
if (ret7 != HAL_OK ) {
strcpy((char*)buf7, "Error Rx\r\n");
}else {
H0_rHx2= buf7[0];
H0_rH= H0_rHx2 / 2;
}
}
//4-H1_rHx2
buf8[0] = REG_H1_rH;
ret8= HAL_I2C_Master_Transmit(&hi2c1, ADDR, buf8, 1, HAL_MAX_DELAY);
if (ret8 != HAL_OK) {
strcpy((char*)buf8, "Error Tx\r\n");
} else{
ret8 = HAL_I2C_Master_Receive(&hi2c1, ADDR, buf8, 2, HAL_MAX_DELAY);
if (ret8 != HAL_OK ) {
strcpy((char*)buf8, "Error Rx\r\n");
}else {
H1_rHx2= buf8[0] ;
H1_rH= H1_rHx2 /2;
}
}
C1= H1_rH-H0_rH;
C2=H_OUT-H0_T0_OUT;
C3=C1*C2;
C4=H1_T0_OUT-H0_T0_OUT;
C5=C3/C4;
HUM=C5+H0_rH;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-29 06:27 AM
Hi @MBalu.1​ , can you please be more specific on the error (code) you are getting? Just to understand if you are missing the I2C communication with the HTS221 sensor (you can check it reading the WHO_AM_I register), or you are reading wrong raw data, or it is a matter of code computation. I can suggest you the C libraries on github for the HTS221 part number (LINK), especially the hts221_read_data_polling.c example. I added STM32G4 tag for broader support from STM32 products' experts. Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-30 01:54 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-06-30 02:15 AM
Hi @MBalu.1​ , and which values do you get? You should get something like 50% rH or similar value, I guess... In this technical note TN1218 you can check how to interpret humidity and temperature readings in the HTS221 digital humidity sensor. Regards