cancel
Showing results for 
Search instead for 
Did you mean: 

Hi I'm testing Unicleo & IKS01A2 for the first time, the software does not recognise any nucleo boards (F401RE & L476RG). If I "list all COM ports" I can connect but the board and firmware is stated unknown. I use Win10, any hints?

FZ
Associate II

0690X000008aDUDQA2.png0690X000008aDTzQAM.png

5 REPLIES 5
Miroslav BATEK
ST Employee

Hello,

You have to program your Nucleo board with one of the application or DatalogExtended example. You can find all applications and examples in X-CUBE-MEMS1 package.

Eleon BORLINI
ST Employee

Hi FZ, did you already installed the STM32 drivers (https://www.st.com/en/development-tools/stsw-stm32102.html)? Regards

FZ
Associate II

Yes I have Atollic and the latest ST Cube IDE, tested the boards and they work in that environment,

I got the MEMS package, I'm I supposed to compile any of the example projects and flash before i launch Unicleo?

Miroslav BATEK
ST Employee

Yes, if you want, for example, to test the sensors on IKS01A2 you can start with DatalogExtended firmware. There is already compiled binary file which you can use, just program the board with the binary file.

FZ
Associate II

Got it running, Thanks!