2020-10-21 08:27 AM
2020-10-23 02:45 AM
Hi @DLomu.1 ,
please note that the FW that sends the sensor data on the cloud, i.e. the FP-IND-PREDMNT1 function pack, does manage the MLC of the ISM330DHCX.
The only FW running on the STWINKT1 that currently manages this feature is the HSDatalog example (in the STSW-STWINKT01 pack), but in this case data are sent on the SD card or via USB to the logging application.
This because the MLC is designed to run on the Edge, but cannot exclude that the requested feature will be implemented in the future FW pack and dashboard releases.
-Eleon