2023-05-15 02:28 PM
2023-05-17 06:45 AM
Hi @cjaya.2 ,
Look at our LPS27HHTW or ILPS28QSW water-resistant MEMS pressure sensor combines chemical compatibility, stability, and accuracy for use in a wide range of applications. Gel inside the IC protects the electrical components from water and the metal cap is grounded electrically for better ESD robustness.
LPS27HHTW also embeds a temperature sensor to monitor ambient temperature, while in ILPS28QSW an embedded Qvar (electric charge variation detection) channel can be enabled for sensing in applications such as water-leak detection, tap, double tap, long press, and L/R - R/L swipe.
You can find more details at this link for LPS27HHTW or here for ILPS28QSW .
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster 🙂