cancel
Showing results for 
Search instead for 
Did you mean: 

Getting started with STEVAL-MIC007V1

OsBo
Associate

Hi Everybody,

 

I am a beginner and I need some information to start using the following devices:

- Nucleo-F401RE

- X-Nucleo-Amicam1

- Steval-mic007v1.

 

I have currently downloaded the following material:

- X-cube-memsmic1

- Link007

- Link009

- Stm32cubeid.

Is it necessary to install additional software tools and/or embedded software?

 

Is it possible to get an initialization procedure or a video guide for the correct configuration of the devices for the use of the Steval-mic007v1 microphones?

 

Thanks for your help.

 

Best wishes,

 

Oscar

 

1 REPLY 1
SimonePradolini
ST Employee

Hello @OsBo 

X-NUCLEO-AMICAM1 + STEVAL-MIC007V1 is natively supported in X-CUBE-MEMSMIC1 in conjunction with NUCLEO-L476RG and NUCLEO-L4R5ZI only. 

By using the above-mentioned setup, you can go through the AMICAM1/Microphone_Streaming examples available in X-CUBE-MEMSMIC1. All the details are available in the User Manual.

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.