2020-05-14 05:16 AM
Hello,
I have a question to the STEVAL-BCN002V1B.
I try some BLE-Examples and flash the bord with some firmware example from the SDK.
Now I can't pair the board with my mobile phone ST APP. Which firmware do I have to use to get the default factory settings back.
Thanks a lot for your support.
Cheers Max
Solved! Go to Solution.
2020-05-14 06:01 AM
Oh now it works.
I used the BLE_SensorDemo_Use_OTA_ServiceManager.hex file
2020-05-14 06:01 AM
Oh now it works.
I used the BLE_SensorDemo_Use_OTA_ServiceManager.hex file
2020-05-14 06:05 AM
Hi @MMaie.1 , you can first try to interface the BCN002V1B with Unicleo-GUI, to check the BLE connectivity on a device that can run Unicleo and is provided by a BLE module. Or, alternatively, you can use the STBLESensor app on your smartphone. To "get back" to a factory tested FW I suggest you to flash an original BLE example such as the BLE_SensorDemo.bin file, that you can find in the\Firmware\BLE_Examples folder of the STSW-BLUENRG1-DK. For this purpose ou can use an ST-LINK/V2 programmer and the STM32Cube Programmer. Regards