cancel
Showing results for 
Search instead for 
Did you mean: 

''gcc'' not found in PATH

Dilbert K
Senior
Posted on October 17, 2017 at 23:12

I am trying the 'STM32CubeExpansion_BLE1_V3.2.0' to build the BLE expansion board 

However I got the build error for project :

STM32CubeExpansion_BLE1_V3.2.0\Projects\Multi\Applications\SensorDemo\SW4STM32\STM32F401RE-Nucleo

When I tried another project, then it is OK.

STM32CubeExpansion_BLE1_V3.2.0\Projects\Multi\Applications\SampleAppThT\SW4STM32\STM32F401RE-Nucleo

Anyone has quick idea what are missing in the IDE project file ??

2 REPLIES 2
Posted on October 18, 2017 at 03:04

Review the project metadata in a file viewer. Not sure they are sufficiently similar to diff, but perhaps look for keywords like path, eabi or gcc

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Dilbert K
Senior
Posted on October 18, 2017 at 04:09

Found the problem after comparing to previous ST projects.

In ToolChainEditor : The '

CDT internal builder

' was selected in this package,  after changing to '

Gnu Make Builder

', it build OK.

Yet to validate the others functionality