cancel
Showing results for 
Search instead for 
Did you mean: 

Driver Example for LIS3DH

Thiago REIS
Associate II
Posted on December 09, 2013 at 13:14

Hello to all,

In order to ease the self learning process and set up ST's LIS3DH, attached to this post is an example of the drivers setup for a general application.

Thank you,

Thiago Reis

#lis3dh #setup
4 REPLIES 4
Mich1
Associate III
Posted on December 16, 2013 at 15:04

what about SPI_Mems_Init();   ???

aritzmartikorena
Associate
Posted on July 03, 2015 at 11:10

Many thanks for the example, however, there is nothing on it regarding the LIS3DH configuration.

Arna Lee
Associate II
Posted on March 07, 2018 at 05:05

Is there a Driver Example for LIS3DH with I2C interface?

Posted on March 07, 2018 at 14:28

We have GitHub repository with sensor drivers.

https://github.com/STMicroelectronics/STMems_Standard_C_drivers

 

Unfortunately LIS3DH is not there but you can check the LIS2DH12 it is very similar device.