‎2019-03-30 2:35 PM
Does the Sensor data logging works for Time of Flight data as well in STEVAL-BCNKT01V1
(bluecoin)?If no how it can be logged?Which file to look for in the workspace?I just need proximity and No Proximity data when bluecoin is mounted on the cradle.
Br,
‎2019-04-01 6:51 AM
hi, do you refer to Sensor data logging of the Android/iOS APK (ST BLESensor app)? If so, you can try to acquire ToF data by flashing the FP-SNS-FLIGHT1 (https://www.st.com/en/embedded-software/fp-sns-flight1.html) on the Bluecoin MCU
Regards
‎2019-04-01 10:31 AM
Thanks for the quick reply.
Is there a way to log the simultaneous data for both ToF and Motion Sensors? I guess FP-SNS-FLIGHT will enable the logging option for ToF only while FP-SNS-ALLMEMS1 for Motion sensors?
Can I get both?which f/w?
Also Bluecoin doesnt have a ToF right?It is on the cradle?Neither on the coin station?
Many thanks in advance !
‎2019-04-01 10:32 AM
sorry i should have replied in the 'reply' instead of a new Answer ! :(
‎2019-04-02 6:36 AM
Don't worry =)
The FP-SNS-FLIGHT1 is able, as per the description, to perform sensor data reading, motion algorithm features demo, proximity-based hand gesture detection demo and firmware update (FOTA). You can fint the FW to be uploaded on the Bluecoin inside the folder:
en.fp-sns_flight1_firmware.zip\STM32CubeFunctionPack_FLIGHT1_V3.3.0\Projects\Multi\Applications\FLIGHT1\EWARM\STM32F446RE-BlueCoin
Regards