2020-06-21 03:56 AM
Have been working with magnetometers for the car parking application. the previous sensors used has not satisfied the range for the application required. Does LSM303 detect at a range of 30cms?
2020-06-22 08:55 AM
Hi @BRaj_48 , as I can see from the BMM150 sensor datasheet, the magnetometer dynamic range is ±13 gauss on x and y axis and ±25 gauss along z axis, while the sensitivity is 3 mgauss/LSB. On the other hand, the LSM303AGR magnetometer part has a wider dynamic range (±50 gauss), while the minimum detectable signal is 1.5mgauss. The LSM303AGR capability is higher both in terms of Full Scale and resolution, so I believe that it can be cover your application requirements. Regards
2020-06-22 10:51 PM
Thank you for your time @Eleon BORLINI, and i have an another doubt as which will have the capability to detect maximum distance is it milli-tesla or the micro-tesla(as the dynamic range)?
2020-06-25 03:29 AM
Should be some tenth of mT... Regards