2022-09-14 11:40 PM
LIS331DLHTR,
The first line is tracking code,
The second line represent the chip,
The third line represent the date code.
2022-09-15 06:36 AM
Hi @AUlan.1 ,
The first line is the date code, in particular the meaning of 2303 is: "2", meaning 2022; "30" is the assy week, 3 is the progressive number for the lot of that week.
The second line is correctly the part number.
The third line an the alphanumeric trace code.
-Eleon