2020-06-30 11:42 AM
Tried redoing the project several times - other labs seem to work
2020-07-02 07:28 AM
Hi @JTrez.1 , do you refer to this section of the training? --> https://www.youtube.com/watch?v=88exXyZ6zxQ&list=PLnMKNibPkDnGsEvFISX3zEb23vLwl8qoN&index=3 can you please be more specific about the project you are referring to? Regards
2020-07-03 12:24 PM
Thanks for the reply. Lab 3 is in the 7th video - Part 7: Lab 3 - LSM6DO XL embedded step counter
https://www.youtube.com/watch?v=DHt9lPjgOIk&list=PLnMKNibPkDnGsEvFISX3zEb23vLwl8qoN&index=7
Let me know if you need sections of the generated code.
2020-07-03 04:50 PM
Update - I redid the Lab from scratch in a new folder with a new name and was able to get it to work. Eventually it did fail again with a hard fault on line 84! It ran again later on after disconnecting usb and restarting the debugger. I am thinking this might be a hardware issue on my board.
2020-07-03 06:40 PM
Can you post any of the debug error data that you are getting when the error is seen? Perhaps from the Console or Debugger Console output?
2020-07-05 05:26 PM
The problem occurs intermitently now. I captured output from the debugger console when it failed:
Temporary breakpoint 1, main () at ../Core/Src/main.c:75
75 HAL_Init();
Program received signal SIGTRAP, Trace/breakpoint trap.
HardFault_Handler () at ../Core/Src/stm32l4xx_it.c:84
84 {
line 83 is: void HardFault_Handler(void)
2020-07-05 06:31 PM
Have you double checked that your are using interrupts [9:5] and pin PB5 for the sensor? This would be around 5:19 in the video.
2020-07-06 11:11 AM
Yes - that is how it is configured. I can rerun the debugger, downloading new code and it will sometimes fail or other times run correctly. This leads me to believe there is a hardware issue causing intermittent behavior. Software always runs correctly or not :)
2020-07-06 12:43 PM
Yeah, strange. Were you able to complete the other labs?
I would check the connection between the NUCLEO-L476RG and X-NUCLEO-IKS01A3 boards or check for some issue like cold solder on the X-NUCLEO-IKS01A3.
However, in my case I used a NUCLEO-L152RE though.
2020-07-06 02:48 PM
All of the other labs worked with no issue. I plugged and unplugged the MEMS board a few times and examined the pins. Cold solder joint is a possibility for that component. Now that I have completed the course, I am OK but will consider the one sensor suspect for future labs or experiments. Thanks for your help.